T1040 debug with Codewarrior PA10.3.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040 debug with Codewarrior PA10.3.3

T1040 debug with Codewarrior PA10.3.3

T1040 is new to all the customers. The ecosystem is still not mature in this moment in Jan'2014

The note is for someone who is using Codewarrior PA10.3.3 for T1040 platform board bring up or debugging on this moment.

if you have problem to connect T1040 platform with Codewarrior, the document might help you.

ラベル(1)
添付
コメント

A couple of comments based on local experience

  • if you run the CWTAP inside the FSL net, it is more convenient to leave it on DHCP. After a few minutes the FSL DNS will pick it up as "fsl<last3bytesmac>", e.g., "fsl023ab3" if the TAPs MAC address ends with 02:3a:b3 per the sticker on the back. This avoids a whole lot of painful IP reconfigurations
  • I believe it is unwise to use the "-force" option when updating the tap's firmware and there must be very good justification to even think about it. The command is smart enough to do the right thing and hasn't failed on me yet.
評価なし
バージョン履歴
最終更新日:
‎01-23-2014 08:41 PM
更新者: