Suggest CodeWarrior IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggest CodeWarrior IDE

1,366 Views
manjunathk
Contributor I

Hi Support team,

 

Could you please suggest me suitable CodeWarrior IDE for S70GL02GS NOR flash and T2080 processor support.

 

Regards,

Manju

Labels (1)
0 Kudos
Reply
1 Reply

1,282 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Manjunath K,

The reccomended Codewarrior version for the T2080 processor is the following:

CodeWarrior Dev Tools for Power Architecture|Freescale

At the bottom of the page you will find a table that shows which capabilities are provided for various boards and processors. The version of CodeWarrior and required service packs are also indicated for each entry. For each board listed, CodeWarrior provides initialization files.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply