Suggest CodeWarrior IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suggest CodeWarrior IDE

1,418件の閲覧回数
manjunathk
Contributor I

Hi Support team,

 

Could you please suggest me suitable CodeWarrior IDE for S70GL02GS NOR flash and T2080 processor support.

 

Regards,

Manju

ラベル(1)
0 件の賞賛
返信
1 返信

1,334件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Manjunath K,

The reccomended Codewarrior version for the T2080 processor is the following:

CodeWarrior Dev Tools for Power Architecture|Freescale

At the bottom of the page you will find a table that shows which capabilities are provided for various boards and processors. The version of CodeWarrior and required service packs are also indicated for each entry. For each board listed, CodeWarrior provides initialization files.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信