Suddenly: Unknown target type

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suddenly: Unknown target type

4,173件の閲覧回数
ddpd
Contributor III

I was working with the projects in code warrior ide.

The same IDE when I started today is displaying some error.

I have attached the screen shot of that error. With this error I cannot debug or the flash the code, but I am able to compile the code.

 

Please let me know what has happened suddenly for the code warrior to behave in this manner.

Thanks in advance.

131441_131441.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,630件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hmm, to me it seems like your installation got corrupted somehow.

I would try to install a new instance of CodeWarrior (you don't have to uninstall your current version) and try if this helps?

Erich

3,630件の閲覧回数
ddpd
Contributor III

Yeah Erich.

You are right.. It seems to be that the IDE has corrupted.

Thanks for your suggestion

0 件の賞賛
返信