Sector Protection Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sector Protection Error

2,002件の閲覧回数
wangjin
Contributor I

My board is P2040NXN7MMC , Code Warrior 10.5, use flash programmer download bootrom in NOR Flash(S29GL01GP). this is a error happened.

Error is :

Error: Erase failed . Flash driver reports the following error(s): Sector Protection Error.

I don.t know why ? I build SRAM Project.

There is someone can help me ? Please

0 件の賞賛
返信
1 返信

1,831件の閲覧回数
Pavel
NXP Employee
NXP Employee

Unprotect your Flash using CodeWarrior. See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信