SPI CS active through a write and read cycle?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI CS active through a write and read cycle?

1,731件の閲覧回数
marknordstrand
Contributor III

MK20DN512VLQ10 with CW 10.4. 

 

Connected to flash which needs CS asserted through the command, address (both writes), and the reading of the data.  I don't see a way to do this with SPIMaster_LDD short of taking over CS as a GPIO and controlling it directly.  Is this correct, or am I missing something?

ラベル(1)
0 件の賞賛
返信
1 返信

1,558件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Mark:

There are some issues with the PE SPI driver (not really bugs, but deficiencies). You can find workarounds and more details in the next thread from the Freescale community:

https://community.freescale.com/thread/307520

==================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信