SPI CS active through a write and read cycle?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI CS active through a write and read cycle?

1,790 Views
marknordstrand
Contributor III

MK20DN512VLQ10 with CW 10.4. 

 

Connected to flash which needs CS asserted through the command, address (both writes), and the reading of the data.  I don't see a way to do this with SPIMaster_LDD short of taking over CS as a GPIO and controlling it directly.  Is this correct, or am I missing something?

Labels (1)
0 Kudos
Reply
1 Reply

1,617 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Mark:

There are some issues with the PE SPI driver (not really bugs, but deficiencies). You can find workarounds and more details in the next thread from the Freescale community:

https://community.freescale.com/thread/307520

==================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply