SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK

3,415件の閲覧回数
buqing_niu
Contributor I

 之前我更新过sdk 到最新版本,但是 新建项目时候,却发现没有 sdk10.0版本的,我怀疑我没安装好,我重新安装,但是提示我 如下:

An error occurred while collecting items to be installed
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,com.jcraft.jsch,0.1.54.v20170116-1932
No repository found containing: osgi.bundle,javaewah,1.1.6.v20160919-1400
No repository found containing: osgi.bundle,org.eclipse.cdt,9.2.1.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.build.crossgcc,1.1.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.build.gcc.core,1.0.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.checkers,3.2.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.checkers.ui,3.2.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.core,4.0.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.core.cxx,3.4.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.ui,3.2.0.201703062208
No repository found containing: osgi.bundle,org.eclipse.cdt.codan.ui.cxx,3.3.0.201703062208

附件中可以看到 截图,之前我也 下载demo板子成功过。但是现在 我不知怎么解决!

ラベル(1)
0 件の賞賛
返信
1 返信

3,296件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

from your original post, I have no idea what would you like to do and which version of S32DS you use.

Could you please clarify the version and what would you like to achieve?

From the figures you shared it looks like you tried to update the IDE by clicking Check for Updates in Help menu. But this is not correct way. If you want to install newest S32DS update, please follow the instructions below (these are for S32DS Power Architecture 2017.R1)

S32 Design Studio for Power Architecture 2017.R1 - Update 10 available 

If you use different version, please see link below and choose appropriate version.

https://community.nxp.com/community/s32/s32ds 

Regards,

Martin

0 件の賞賛
返信