S12ZVML-MINIBRD and LINUX Driver.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVML-MINIBRD and LINUX Driver.

2,250件の閲覧回数
arieleo
Contributor I

Hi. I'm new in S12ZVML-MINIBRD development. I need it to control a Brush motor. But I need to use linux for my application control. Is it a linux driver distribution or a library for this purpose?

Thanks.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,058件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

FreeMaster is Real Time Monitor and Control Panel, but it is also for windows only.

As I know, NXP doesn't have active SW tool for S12Z on linux.

Our recommend application is S12ZVML-MINIBRD_BLDC, but it's not for linux.

https://www.nxp.com/downloads/en/apps/S12ZVML-MINIBRD_BLDC.exe 

For more information, refer

S12 MagniV Mini Board for Motor Control|NXP 

Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,058件の閲覧回数
arieleo
Contributor I

Then is it impossible to send commands since a Linux platform to S12ZVML-MINIBRD device in order to control a bdlc motor?

Thanks.

0 件の賞賛
返信

2,058件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

As I know, we don't have linux driver distribution.

Best Regards

Jennie Zhang.

0 件の賞賛
返信