S record

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S record

2,304件の閲覧回数
haroldvogel
Contributor II

How do I get CodeWarrior to generate an S Record file for release to the customer?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,131件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Harold

Please open the project properties, and go to the settings for link options, enable the option “S-record generation”.

Hope this helps!  If not, please reply with the CodeWarrior version you are using, and the part number of your MCU.

For Classic CodeWarrior, please:

1)Start the IDE and click on Help | About Freescale(Metrowerks) CodeWarrior.

2)Click on Installed Products

3)Provide us all info displayed. Or you can save them in a txt file.

For Eclipse CodeWarrior, please:

1)Start the IDE and click on Help | About CodeWarrior Development Studio.

2)Provide us the info displayed.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,131件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Harold,

the answer depends on which toolchain you are using.

For example for ARM, https://mcuoneclipse.com/2012/09/13/s-record-generation-with-gcc-for-armkinetis/  shows how to use the build tool settings to generate an S19 file.

For S08/S12 in CodeWarrior, you could use this: https://mcuoneclipse.com/2013/10/29/s-record-manipulation-with-gnu-objcopy-and-burner-utility/

There is as well this way: https://mcuoneclipse.com/2012/09/27/s-record-intel-hex-and-binary-files/

If you want to use a powerful tool for S-Record manipulation, I'm using the 'Srecord' tool, described in https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/  and https://mcuoneclipse.com/2016/02/26/merging-s19-files/

I hope this helps,

Erich

0 件の賞賛
返信

2,131件の閲覧回数
haroldvogel
Contributor II

Thank you all.  I have found the selection under the Prosperities to select s-record output.

0 件の賞賛
返信