Remove project path from glo file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Remove project path from glo file

2,180 Views
michthom
Contributor II

Hi,

 

i would like to know how to generate a glo file with no project path line.

 

The purpose is to get the exact same binary file wherever I compile it.

 

Thank in advance,

Michel Thomas

Labels (1)
0 Kudos
Reply
4 Replies

2,138 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

if you use CW for HCS12(x), to remove path from s0 record, please follow below steps in project setting.

pastedImage_15.png

can this help you? if not, please port your question here. thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,138 Views
michthom
Contributor II

Hi Jennie,

thank you for the fast reply.

This answers the question.

Regards,

Michel

0 Kudos
Reply

2,138 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome.

If this post answers your question, please click the Correct Answer button. Thank you.

Have a great day,
Jennie Zhang

0 Kudos
Reply

2,138 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Michel

Could you tell us what CodeWarrior version and MCU are you using?

Best regards

Jorge Alcala

0 Kudos
Reply