Remove project path from glo file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Remove project path from glo file

2,073件の閲覧回数
michthom
Contributor II

Hi,

 

i would like to know how to generate a glo file with no project path line.

 

The purpose is to get the exact same binary file wherever I compile it.

 

Thank in advance,

Michel Thomas

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,031件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

if you use CW for HCS12(x), to remove path from s0 record, please follow below steps in project setting.

pastedImage_15.png

can this help you? if not, please port your question here. thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,031件の閲覧回数
michthom
Contributor II

Hi Jennie,

thank you for the fast reply.

This answers the question.

Regards,

Michel

0 件の賞賛
返信

2,031件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome.

If this post answers your question, please click the Correct Answer button. Thank you.

Have a great day,
Jennie Zhang

0 件の賞賛
返信

2,031件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Michel

Could you tell us what CodeWarrior version and MCU are you using?

Best regards

Jorge Alcala

0 件の賞賛
返信