Re: artifact name

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: artifact name

1,935 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Stefano,

 

Could you tell us which MCU and CodeWarrior version are you using?

 

Thanks in advance!

 

Best Regards,

Carlos Mendoza

Technical Support Engineer

标签 (1)
0 项奖励
回复
1 回复

1,739 次查看
stefanomanca
Contributor III

Hi, I can't answer by web.I'm using CW 10.6 and kinetis kl15.Thank you.

-


Messaggio originale----

Da: "Carlos_Mendoza" <[email protected]>

Data: 30/05/2016 17.59

A: "stefano manca"<[email protected]>

Ogg: Re: - artifact name

a

body {

font-family: Helvetica, Arial, sans-serif;

-webkit-text-size-adjust: 100%;

}

h1, h2, h3, h4, h5, h6, p, hr {

-webkit-margin-before: 0;

-webkit-margin-after: 0;

-webkit-margin-start: 0;

-webkit-margin-end: 0;

}

.button td {

background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0 51%, #387AC8 100%) !important;

background-image: -webkit-gradient(linear, left top, left bottom, color-stop(0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#387AC8)) !important;

-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

}

-->

NXP Community

artifact name

reply from Carlos_Mendoza in CodeWarrior Development Tools - View the full discussion

Hi Stefano,

Could you tell us which MCU and CodeWarrior version are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Development Tools by email or at NXP Community

Following artifact name in these streams:

Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 项奖励
回复