ROM -out of allocation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ROM -out of allocation

1,303 Views
karunanithiprat
Contributor II

Hi, I am using MC9RS08LA8 controller with code warrior 6.3. I have to add some functions in existing program and i have 300 bytes of ROM memory. When i add one 32 bit division operation it showing out of allocation space in ROM. why and how its happening? i  have added just one line division (ex: signed long Variable1; Variable1=Variable1/100u;)

Thanks,

Labels (1)
0 Kudos
Reply
1 Reply

1,150 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

the answer can be referred from this thread:

ROM allocation exceed-MC9RS08LA8


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply