Problem with MPC5748G programming using ic5000 from iSYSTEM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with MPC5748G programming using ic5000 from iSYSTEM

2,067 Views
medhedibasly
Contributor III

Hello,

I'm working with MPC5748G and ic5000 Debugger with WInIDEA.

Sometimes when i try to reprogram my board (custom board) with new application the board get stuck and i can't download the new application. I tried to erase th flash by performing a mass erase operation, WinIDEA says that the mass erase has successfully passed but the flash is not erased.

Any explanation or a way to explore more this issue would be appreciated.

best regards,

Hedi.

0 Kudos
Reply
2 Replies

1,881 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hedi

ic5000 Debugger and WInIDEA are both iSYSTEM product. I would suggest you contact iSYSTEM:

iSYSTEM - iSYSTEM - Enabling Safer Embedded Systems 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,881 Views
medhedibasly
Contributor III

Hi Jennie,

Thank you for your response, i will contact iSYSTEM to discuss the issue with them.

Best regards,

Hedi.

0 Kudos
Reply