Problem while installing the codewarrior 8.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem while installing the codewarrior 8.8

1,755 Views
maheshwarreddy
Fresh Out Contributor

Now we are using the MPC860 power pc in our custom board. To dbug we are trying to use the code warrior 8.8 but while installing the code warrior we are getting an error as cannot not run an x86 built of this utility on x64 platform. How to solve this . The installing PC will be 64 bit .

Thank you 

Best regards 

Maheshwar

0 Kudos
Reply
1 Reply

1,656 Views
Pavel
NXP Employee
NXP Employee

There is similar message during CodeWarrior 8.8 installation.

Install "Software Patch: CW PA v8.8.6 Windows" after CodeWarrior 8.8 installation. See the following page:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121541

 

This patch installs driver for CodeWarrior TAP.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply