supported code warrior version for the MPC860 power pc with processor ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

supported code warrior version for the MPC860 power pc with processor ?

1,634件の閲覧回数
ravadasrikanth3
Fresh Out Contributor

we are using MPC860 processor . we are unable to found the device itself in codewarrior 10.5.1. so which version of the code warrior IDE supported.

Thank you

Best regards

0 件の賞賛
返信
1 返信

1,546件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 for the MPC860. This CodeWarrior is available on the following page:

https://nxp.flexnetoperations.com/control/frse/product?child_plneID=691401&ver=CURRENT

 

Install also "Software Patch: CW PA v8.8.6 Windows". See the following page:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121541

 

This patch installs driver for CodeWarrior TAP.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信