Print settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,173件の閲覧回数
pascalschröer
Contributor V

Hi at all,

 

Can anyone tell me, how to set up some print settings in CW10.6?? I would like

to set up the distance between the code and the page borders... The "normal"

printer settings don't have options like that.

 

Thanks!

 

 

Pascal

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,068件の閲覧回数
pascalschröer
Contributor V

Now, I have solved the problem! There isn't an option to set up the side clearance, so you have to

scale down the printed window!

Thanks

Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,068件の閲覧回数
catalindemergia
Contributor IV

Hi,

After File->Print, select your printer and then hit the Preferences button,

you will find all the settings there.

regards,

Catalin

print_settings.png

3,068件の閲覧回数
pascalschröer
Contributor V

Hey,

Ok I have seen this settings but I can't set up the side clearance... Do you know

a solution for this problem?

Thanks!

Pascal

0 件の賞賛
返信
3,068件の閲覧回数
pascalschröer
Contributor V

Now, I have solved the problem! There isn't an option to set up the side clearance, so you have to

scale down the printed window!

Thanks

Pascal

0 件の賞賛
返信