Planning to replace SPI flash (N25Q128A) with MT25QL512ABB is there any driver dependency?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Planning to replace SPI flash (N25Q128A) with MT25QL512ABB is there any driver dependency?

2,075 次查看
sarath_gs
Contributor II

I am using NXP K60 processor now it is interfaced with 16MB (4KB Sector Erase N25Q128A) external SPI flash . i am planning to  update the flash size up to 64MB (4KB, 32KB, 64KB, Sector Erase MT25QL512ABB) is need any SPI driver modifications? 

0 项奖励
回复
1 回复

1,982 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

I am so glad to serve you. 

As you mentioned, the flash has been updated to 64MB, and the first point is change the "#define flash_size  xxxx".And there may has some other cmd ,you can add the cmd to the head file for useing. And new cmd could be packed into a new fuction. For more difference,please refer to the RM and datasheet.

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复