Pass struct to function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pass struct to function

4,520 次查看
tnriley
Contributor III

I seem to be having some difficulty in passing a struct to a function. No errors generated by the make process but upon inspection the values inside the function are not equal to the values outside.

 

 

THE STRUCT:

struct sciData{
  uint8_t rxBuf[RSBuffSIZE]; // Receive buffer
  uint16_t RSindex; // receive buffer counter
  uint16_t RSread; // receive buffer counter

  uint32_t tempVal; //scratchpad calc storage space
  uint8_t tempChars[TBUFF_SIZE]; //temporary scratchpad for received chars
  //Data Transmit Parameters
  uint8_t txBuf[SendBuffSIZE]; /* Send buffer */
  uint16_t numTXBytes;
  uint16_t OutBytes; /* Number of bytes to send */
  uint16_t SentBytes; /* Number of bytes sent */
  uint16_t TRANSMIT; // transmit flag to let prog know interrupt
  // driven transmission in progress
  uint8_t tPtr; //pointer to current buffer item
  uint8_t dataReady; //flag to indicate return data ready
  uint8_t charCount; //number of chars received
  uint8_t commChar;
  uint16_t charsExpected;
};

 

 

STRUCT DEFINE IN MAIN:

struct sciData sci3Dat;

 

CALL FROM MAIN

//Send Mode change to Top Controller
sci3Dat.txBuf[0] = 'p';
sci3Dat.txBuf[1] = 'G';
sci3Dat.txBuf[2] = TC_START;
sci3Dat.numTXBytes = 3;

  (NOTE: At this point sci3Dat.numTXBytes = 3)

#ifdef SCI3
  SendSerialData3(&sci3Dat); //past end of data
  while(sci3Dat.TRANSMIT);
#endif

 

 

INSIDE THE FUNCTION:

/* routine called to start string transmission */
void SendSerialData3(struct sciData *sd3){
        (NOTE: At this point sd3->numTXBytes = 0)

   sd3->OutBytes = sd3->numTXBytes - 1;
   sd3->SentBytes = 0;
   sd3->TRANSMIT = 1; // We're transmitting data

   /* Set transmit buffer empty * transmit complete interrupts */
   INTR_OFF();
   SCI3CR2 = 0xEc;
   INTR_ON();
}

 

Other values are incorrect also, just included the numTXBytes as an example. Pointer to a function should be fairly simple right, but I am not sure where I have gone wrong here.

 

Any Ideas?

标签 (1)
7 回复数

4,287 次查看
tnriley
Contributor III

Stan,

Thanks, I will try that. I am new to the Codewarrior tools.

I set the project up with the small memory model option. Which I thought meant that it was a non paged contiguous space. What is the best source for documentation on learning and using the different memory models for CodeWarrior and the MC9S12?

Tim

0 项奖励
回复

4,287 次查看
stanish
NXP Employee
NXP Employee

Hi,

Not sure which memory model you are using, but perhaps this issue is related to the fact your struct is located in a paged RAM and the function call doesn't pass the page number.

I'd suggest you to declare sciDATA pointer as a far pointer so it passes global address pointer instead:

void SendSerialData3(struct sciData  *far sd3)

Hope it helps.

Stan

0 项奖励
回复

4,287 次查看
tnriley
Contributor III

Alice,

How is best to post files here?

Tim

0 项奖励
回复

4,287 次查看
tnriley
Contributor III

Alice,

The chip is a Freescale MC9S12XDP512CAL. The CodeWarrior IDE version is 5.9.0 build 5294.

Sorry, I can't send the complete project.

Thanks,

Tim

0 项奖励
回复

4,287 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tim,

OK, it doesn't matter.

I create a new project about it , and copy these code into it , while when build there some error,

as to lack of some definition , for example INTR_OFF()...

So could you please also create a new project , then only copy these code related your question,

build with no error, check whether it can work well . If no, please share it to me this project .

BR

Alice

0 项奖励
回复

4,287 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tim,

Please tell me the chip part number and the version of CodeWarrior.

Also in order to check the problem , please share your project t me , thanks.

BR

Alice

0 项奖励
回复

4,287 次查看
tnriley
Contributor III

I was looking at this some more and found the following

The value of sd3 inside the function void SendSerialData3(struct sciData *sd3) is reported as sd3=NULL by the Codewarrior IDE.

Whereas the value of sd3 in the function void out_serial3(struct sciData *sd3) (Shown Below) points to the correct struct sci3Dat defined back in main(). 

 

INSIDE THE FUNCTION CALLED BY THE ISR:

/* Send data routine. Called by sci interrupt handler */
void out_serial3(struct sciData *sd3){
   if(sd3->SentBytes > sd3->OutBytes){ // if last character transmitted
      INTR_OFF(); // turn off transmitter interrupts
      SCI3CR2 = 0x24; // Also turns off transmitter when last char is sent
      sd3->TRANSMIT = 0; // notify main program that tranmission is complete
      INTR_ON();
   }
   else
      SCI3DRL = sd3->txBuf[sd3->SentBytes++]; // stuff character in sci transmit buffer
   }

ISR SHOWING CALL TO out_serial3

/* interrupt handler for all SCI3 communications interrupts */
void interrupt com3(void){
   uint8_t scitest = SCI3SR1;
   if(scitest&BM_RDRF){ // if receive buffer full interrupt, call data receive routine
      in_serial3(&sci3Dat);
   }
   else{
      if(scitest&(BM_TDRE|BM_TC)){ // if transmit buffer empty or transmit complete interrupt,
         out_serial3(&sci3Dat); // call transmit data routine
      }
   }
}

 

The code for all three modules SendSerialData3, out_serial3, and com3 reside in the same file.

 Parameters to both modules are defined in the same manner (struct sciData *sd3) and calls are made in same fashion (&sci3Dat).

So the question is:  Why does sd3=NULL inside SendSerialData3, but contain the correct values inside out_serial3?