P1010RDB-PB_init_sram.tcl Init Failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010RDB-PB_init_sram.tcl Init Failed

1,741件の閲覧回数
yongleo_
Contributor I

Dear all!

I tried connect to the p1010NXN5HHB target board in SRAM mode in the CW10.5.1 environment using the p1010RDB_PB DEMO  program. JTAG can initialize successfully. But when initializing the "/CFG/P1010RDB-PB_init_sram.tcl" file, "Error message: ELF not in expected HALT mode" Problem occurred .

200186_200186.jpgIMG_20171011_163613.jpg

200187_200187.jpgIMG_20171011_154746.jpg

I'd welcome any suggestions.

Original Attachment has been moved to: p1010-pb-core00.rar

Original Attachment has been moved to: log1.txt.zip

Original Attachment has been moved to: log.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,627件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached file.

Do you use the same configuration for using P1010 SRAM?


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信