求高手指教:HC908jk 这款芯片有没有C代外设码库,或者在哪里可以找到C代码的例子啊,
第一次用飞思卡尔的片子,这款芯片可能年代较久远,在官网上找不到对应的C代码例子,求帮助
Hi
HC908JK is too old. It's hard to find C demo code for this chip exactly.
But you can refer AN2504SW and AN2948SW.
8-bit General Purpose JK and JL MCUs|NXP
AN2504SW is for HC908JL, you can also use it for HC908JK
EY, QY of AN2948SW are both HC08 core as CH908JK, You can refer it to develop HC908JK too.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------