NXP-CUP-Line scan camera issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP-CUP-Line scan camera issues

4,562 Views
mustafashukor
Contributor II

Hello,

I am a participant in the NXP CUP.

The problem is that I can't open line scan camera (linear CCD camera) with the FRDM KL25Z board.

I tried  to open the camera but no success.

WhatsApp Image 2019-02-09 at 22.29.02.jpeg

(the red led does not  mean that the camera is working well?!)

And I checked if the problem was from the serial communication but I send data using the SDA mini usb port successfully.

So I think the problem is in the camera itself, but I do not have any idea how to solve this problem.

Please, I need a solution as soon as possible! 

Thanks in advance.

Labels (1)
4 Replies

4,159 Views
mustafashukor
Contributor II

Solved! as mentioned in the README.pdf file here NXP FRDM-KL25Z Support Package Update - File Exchange - MATLAB Central .

4,159 Views
ondraceq
Contributor I

Hello,

we have encountered what I believe is a similar problem.

We wanted to test the camera on TFC-TEST_UPDATED_HW - Example program that tests CCD1, Servo 1, and b... | Mbed  code from Mbed using FRDM-TFC - Updated TFC library to be compatible with the r... | Mbed  library.

But when we select to print out the input from the camera, it's similar to what we get when we unplug the camera.

Thanks

4,159 Views
mustafashukor
Contributor II

Yes, this random displayed output is the same even if the camera is unplugged, so I think the camera isn't seen by the board.

Did you find any solution? @Ondřej Svoboda 

0 Kudos
Reply

4,159 Views
ondraceq
Contributor I

No, at least not yet.

0 Kudos
Reply