Hi
I use the codewarrior 10.6.4 for programing the MCU with the Multilink Universal.
I have two projects, one is using 9s08PA60 chip,the other is using 9S12XEG128 chip.
Today, when I progarmed the 9s08PA60 chip,the multilink universal firmware updating picture appeared and
installed automatically.
After that , I can't use it to program the 9S12XEG128 chip(the other multilink universal which is not updated is ok).
The error picture is as below.


And how can I change the multilink universal firmware by codewarrior?
I look forward to your reply ,thank you very much!
Jason