Migration from CW to KDS 3.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Migration from CW to KDS 3.2

2,663件の閲覧回数
mayursavaj
Contributor III

Hi Everyone,

We are using CW10.6 for our application development. We want to migrate from CW to KDS 3.2. 

Can anyone help me out to find out how to migrate without changes much.

Regards,

Mayur Savaj

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,463件の閲覧回数
mayursavaj
Contributor III

Hi Alice,

I have followed the process of KDS_Porting_Guide.

When I tried to "Convert CodeWarrior Project file.." isn't working (not going forward).

 

Thanks,

Mayur Savaj

0 件の賞賛
返信

2,463件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur,

I think you  can also create a simple bare board project on KDS, then copy&paste your

application code into KDS project , then build and change some  build error .

BR

Alice

0 件の賞賛
返信

2,463件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

There is a porting guide from CW to KDS under KDS install folder :KDS_Porting_Guide.pdf,

I also attached it.

And also there is a doc about "porting kinets interrupt form CW to KDS":

Porting Kinetis Interrupt from CodeWarrior to KDS  ,  I think you can refer to these two DOCs to port .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信