Migration from CW to KDS 3.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Migration from CW to KDS 3.2

2,729 次查看
mayursavaj
Contributor III

Hi Everyone,

We are using CW10.6 for our application development. We want to migrate from CW to KDS 3.2. 

Can anyone help me out to find out how to migrate without changes much.

Regards,

Mayur Savaj

标记 (1)
0 项奖励
回复
3 回复数

2,529 次查看
mayursavaj
Contributor III

Hi Alice,

I have followed the process of KDS_Porting_Guide.

When I tried to "Convert CodeWarrior Project file.." isn't working (not going forward).

 

Thanks,

Mayur Savaj

0 项奖励
回复

2,529 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur,

I think you  can also create a simple bare board project on KDS, then copy&paste your

application code into KDS project , then build and change some  build error .

BR

Alice

0 项奖励
回复

2,529 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

There is a porting guide from CW to KDS under KDS install folder :KDS_Porting_Guide.pdf,

I also attached it.

And also there is a doc about "porting kinets interrupt form CW to KDS":

Porting Kinetis Interrupt from CodeWarrior to KDS  ,  I think you can refer to these two DOCs to port .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复