Metrowerks Codewarrior sur Windows 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Metrowerks Codewarrior sur Windows 10

2,469 次查看
gfa
Contributor I

Je travaillais pas le passé sur METROWERKS Codewarrior IDE (sous windows XP) pour développer des solutions sur FREESCALE (MOTOROLA) HC912D60A.

Je dois retravailler sur un ancien soft, mais dispose simplement d'un PC sous windows 10.

Les outils de l'époque ne fonctionnent pas.

Comment faire?

Merci

标签 (1)
0 项奖励
回复
1 回复

2,366 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

This device is too old and it is only supported on CW5.1. Please check the video instructions in the thread below to download the IDE.

 

CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2 does not have optio... 

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复