Meaning of "Invalid target system access" error message for CodeWarrior TAP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Meaning of "Invalid target system access" error message for CodeWarrior TAP

2,089 次查看
christiankeller
Contributor II

I have a CodeWarrior TAP connected via USB. The device has worked fine before. Cables have not been changed or disconnected. However upon today's start of the CodeWarrior IDE, the connection seems not to get recognised. Instead the IDE tells me the error message:

 

"Invalid target system access: 'C:\Freescale\CW_PA_v10.5.1\PA\cdde\bin\cdde.exe'"

 

I have no idea what this is supposed to mean. Is there a list of error message for the tooling with a description about its meaning?

 

The connection server does identify the probe correctly with the "findcc cwtap -usb" command.

 

From my experience the connection reliability with the tap and the IDE has been...unstable...to put it politely.

标签 (1)
5 回复数

1,928 次查看
addiyi
NXP Employee
NXP Employee

We are working on this :smileyhappy:

1,928 次查看
addiyi
NXP Employee
NXP Employee

You are trying to use QCVS or Performance Analysis or just a bareboard project?

Adrian

0 项奖励
回复

1,928 次查看
christiankeller
Contributor II

SerDes Line config read in with the Assistant on the ProcessorExpert validation tool.

Same message appears with the DDR settings validation tool, which has worked before.

0 项奖励
回复

1,928 次查看
addiyi
NXP Employee
NXP Employee

Check if any cdde instance is running. Close all ccs/cdde/python process, restart CodeWarrior and check if in Target Connection the path to cdde is correct.

Adrian

1,928 次查看
christiankeller
Contributor II

Thank you, that did the trick! If only the message would be more helpful...

0 项奖励
回复