Hi Duan,
I suggest update to the new firmware that was released on Dev,4.
http://www.pemicro.com/downloads/download_file.cfm?download_id=346
USB Multilink Universal Resource CD (10275 KB)
don't forget use firmware updates tool to update the firmware.
for example, if you work with 8/16bit MCU, you need udate firmware to support RS08/S08/S12(X)(Z)/…, see below screenshot:
 
If the target is PPC5xxx, choose setting as:
Can this help you solve the problem?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Damon
Please install the latest patch on CW6.3 and update with the latest firmware for Multilink Universal:
http://www.pemicro.com/faqs/faq_view.cfm?id=211
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------