MPC566EVB default binaries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC566EVB default binaries

1,739件の閲覧回数
sverhoff
Contributor I

Is there a location where I can find the default binaries for the NXP MPC566EVB development board? I would like to reflash a board that I have acquired to its defaults.

0 件の賞賛
返信
1 返信

1,697件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

default dBUG monitor can be downloaded here:

https://axman.com/content/cme-566 

"User should note that the debug monitor firmware is installed in this flash device.  Development tools or user application programs may erase or corrupt the debug monitor. If the debug monitor becomes corrupted and it’s operation is desired, the firmware must be programmed into the flash by applying a development port tool such as BDM or Nexus. User should use caution to avoid this situation. The upper 1 MByte is used to store the MPC566EVB dBUG debugger/monitor firmware (0x0090_0000 to 0x009F_FFFF)."

Regards,

Lukas

0 件の賞賛
返信