MPC566EVB default binaries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC566EVB default binaries

1,709 Views
sverhoff
Contributor I

Is there a location where I can find the default binaries for the NXP MPC566EVB development board? I would like to reflash a board that I have acquired to its defaults.

0 Kudos
Reply
1 Reply

1,667 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

default dBUG monitor can be downloaded here:

https://axman.com/content/cme-566 

"User should note that the debug monitor firmware is installed in this flash device.  Development tools or user application programs may erase or corrupt the debug monitor. If the debug monitor becomes corrupted and it’s operation is desired, the firmware must be programmed into the flash by applying a development port tool such as BDM or Nexus. User should use caution to avoid this situation. The upper 1 MByte is used to store the MPC566EVB dBUG debugger/monitor firmware (0x0090_0000 to 0x009F_FFFF)."

Regards,

Lukas

0 Kudos
Reply