MCAT tool questions(using MTRCKTSPNZVM128 example)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCAT tool questions(using MTRCKTSPNZVM128 example)

2,104 次查看
bjhwang
Contributor I

Dear Sir or Madam,

Hi this is B.J.

I want to ask you question about this MTRCKTSPNZVM128 example.

Before asking question, here are my development set up.


OS: Win 7(x64)

Development tool : Code Warrior 10.7

                               Freemaster 2.0 (2.0.7)

Debugger tool      :Multilink Universal FX

Example SW        : MTRCKTSPNZVM128.exe(S12ZVM Mixed-Signal MCUs|MagniV|NXP )

All the process works fine(import the sw -> bulid sw -> compile sw).

But the problem is the opening the MCAT Tool program which is included in the example.

After starting the communication, when I want to update the target, it keeps showing the error message.

The error message says, Error - following constants cannot be updated in FM.

Could you tell me what the problem is?

Thank you and have a nice day.

0 项奖励
回复
1 回复

1,994 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi B.J.,

Do you use the latest version of Example SW (REV 1.3)? If not, please try it again with the new version.

Could you please check the java version?

Thank you.

I hope it helps you.

Best regards,

Diana

0 项奖励
回复