MCAT tool questions(using MTRCKTSPNZVM128 example)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCAT tool questions(using MTRCKTSPNZVM128 example)

2,105 Views
bjhwang
Contributor I

Dear Sir or Madam,

Hi this is B.J.

I want to ask you question about this MTRCKTSPNZVM128 example.

Before asking question, here are my development set up.


OS: Win 7(x64)

Development tool : Code Warrior 10.7

                               Freemaster 2.0 (2.0.7)

Debugger tool      :Multilink Universal FX

Example SW        : MTRCKTSPNZVM128.exe(S12ZVM Mixed-Signal MCUs|MagniV|NXP )

All the process works fine(import the sw -> bulid sw -> compile sw).

But the problem is the opening the MCAT Tool program which is included in the example.

After starting the communication, when I want to update the target, it keeps showing the error message.

The error message says, Error - following constants cannot be updated in FM.

Could you tell me what the problem is?

Thank you and have a nice day.

0 Kudos
Reply
1 Reply

1,995 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi B.J.,

Do you use the latest version of Example SW (REV 1.3)? If not, please try it again with the new version.

Could you please check the java version?

Thank you.

I hope it helps you.

Best regards,

Diana

0 Kudos
Reply