MCAT tool questions(using MTRCKTSPNZVM128 example)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAT tool questions(using MTRCKTSPNZVM128 example)

2,102件の閲覧回数
bjhwang
Contributor I

Dear Sir or Madam,

Hi this is B.J.

I want to ask you question about this MTRCKTSPNZVM128 example.

Before asking question, here are my development set up.


OS: Win 7(x64)

Development tool : Code Warrior 10.7

                               Freemaster 2.0 (2.0.7)

Debugger tool      :Multilink Universal FX

Example SW        : MTRCKTSPNZVM128.exe(S12ZVM Mixed-Signal MCUs|MagniV|NXP )

All the process works fine(import the sw -> bulid sw -> compile sw).

But the problem is the opening the MCAT Tool program which is included in the example.

After starting the communication, when I want to update the target, it keeps showing the error message.

The error message says, Error - following constants cannot be updated in FM.

Could you tell me what the problem is?

Thank you and have a nice day.

0 件の賞賛
返信
1 返信

1,992件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi B.J.,

Do you use the latest version of Example SW (REV 1.3)? If not, please try it again with the new version.

Could you please check the java version?

Thank you.

I hope it helps you.

Best regards,

Diana

0 件の賞賛
返信