License problem and no answer from Support from 4 days

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License problem and no answer from Support from 4 days

Jump to solution
4,288 Views
armandjoubert
Contributor I

Hello

First of all, sorry for my bad english, I'm french ...

 

I just installed Codewarrior 6.3 in a new PC (XP 32 bits) because the old PC was stolen.

The installation went well.

I made a new license file with my new disk ID. OK.

 

But when I want to build my project I get an error message:

'Unable to use the plugin "Embedded Coldfire Linker". It is a licensed and a valid license key was not found."

 

But with my old PC and my old license, I did not have this problem.

My project uses a MCF51AC256 Coldfire.

 

I don't know where is my error when I create the license file.

 

I opened a service request, but but I still have not re response support for more than 4 days

 

Can you help me?

 

Thank you

Labels (1)
0 Kudos
Reply
1 Solution
4,187 Views
trytohelp
NXP Employee
NXP Employee

Bonjour Armand,

Pouvez-vous me donner le numéro de votre SR ?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
8 Replies
4,188 Views
trytohelp
NXP Employee
NXP Employee

Bonjour Armand,

Pouvez-vous me donner le numéro de votre SR ?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,187 Views
armandjoubert
Contributor I

Thank's for your answer.

I solved my problem alone, and still no response from support. It is limited as attitude....

0 Kudos
Reply
4,187 Views
trytohelp
NXP Employee
NXP Employee

Ok.

With the SR# I could check/track in the data base to understand what was the problem.

Pascal

0 Kudos
Reply
4,187 Views
armandjoubert
Contributor I

OK : 1-3640782752

Thank's Pascal

0 Kudos
Reply
4,187 Views
trytohelp
NXP Employee
NXP Employee

Thanks.

0 Kudos
Reply
4,187 Views
armandjoubert
Contributor I

Hello,

I have a new problem with my license file

I re-open my SR 1-3640782752  :

I can't use Processor expert (it's in Demo mode), but before (with my old PC and my old license file) I could !.

Someone can help me please ?

Thank's for your help

0 Kudos
Reply
4,187 Views
trytohelp
NXP Employee
NXP Employee

Hi Armand,

I take the SR on my side.

We've a problem with all Classic version license file generated with the new web license system which has been introduced middle of december.

The Processor Expert bean feature is corrupted.

We need to correct and re-encrypt the license file manualy.

Regards

Pascal

4,187 Views
armandjoubert
Contributor I

Thank you Pascal.

It seems to work :smileygrin:

0 Kudos
Reply