License problem and no answer from Support from 4 days

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License problem and no answer from Support from 4 days

ソリューションへジャンプ
4,225件の閲覧回数
armandjoubert
Contributor I

Hello

First of all, sorry for my bad english, I'm french ...

 

I just installed Codewarrior 6.3 in a new PC (XP 32 bits) because the old PC was stolen.

The installation went well.

I made a new license file with my new disk ID. OK.

 

But when I want to build my project I get an error message:

'Unable to use the plugin "Embedded Coldfire Linker". It is a licensed and a valid license key was not found."

 

But with my old PC and my old license, I did not have this problem.

My project uses a MCF51AC256 Coldfire.

 

I don't know where is my error when I create the license file.

 

I opened a service request, but but I still have not re response support for more than 4 days

 

Can you help me?

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
4,124件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Bonjour Armand,

Pouvez-vous me donner le numéro de votre SR ?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
4,125件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Bonjour Armand,

Pouvez-vous me donner le numéro de votre SR ?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,124件の閲覧回数
armandjoubert
Contributor I

Thank's for your answer.

I solved my problem alone, and still no response from support. It is limited as attitude....

0 件の賞賛
返信
4,124件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Ok.

With the SR# I could check/track in the data base to understand what was the problem.

Pascal

0 件の賞賛
返信
4,124件の閲覧回数
armandjoubert
Contributor I

OK : 1-3640782752

Thank's Pascal

0 件の賞賛
返信
4,124件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Thanks.

0 件の賞賛
返信
4,124件の閲覧回数
armandjoubert
Contributor I

Hello,

I have a new problem with my license file

I re-open my SR 1-3640782752  :

I can't use Processor expert (it's in Demo mode), but before (with my old PC and my old license file) I could !.

Someone can help me please ?

Thank's for your help

0 件の賞賛
返信
4,124件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Armand,

I take the SR on my side.

We've a problem with all Classic version license file generated with the new web license system which has been introduced middle of december.

The Processor Expert bean feature is corrupted.

We need to correct and re-encrypt the license file manualy.

Regards

Pascal

4,124件の閲覧回数
armandjoubert
Contributor I

Thank you Pascal.

It seems to work :smileygrin:

0 件の賞賛
返信