LS1046A-FRWY system hangs when CodeWarrior connects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A-FRWY system hangs when CodeWarrior connects

1,414 次查看
mindchasers
Contributor III

Hello,

I'm running the LS1046A Yocto SDK (5.4.3+g134788b16485). It boots fine and mounts its rootfs from the SD Card. When CodeWarrior connects, I get the following message on the terminal and then the terminal hangs.

"EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)"

If I run rootfs from a RAM disk, the system seems to run fine with CodeWarrior.

I'm looking for suggestions on how to resolve this problem. Thank you.

0 项奖励
回复
1 回复

1,409 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Do you want to use CodeWarrior to connect to the target board to do Linux Kernel debugging?

If yes, please refer to CodeWarrior configuration in section 3 in this document.

https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-bo...

0 项奖励
回复