LS1046A-FRWY system hangs when CodeWarrior connects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A-FRWY system hangs when CodeWarrior connects

2,000件の閲覧回数
mindchasers
Contributor III

Hello,

I'm running the LS1046A Yocto SDK (5.4.3+g134788b16485). It boots fine and mounts its rootfs from the SD Card. When CodeWarrior connects, I get the following message on the terminal and then the terminal hangs.

"EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)"

If I run rootfs from a RAM disk, the system seems to run fine with CodeWarrior.

I'm looking for suggestions on how to resolve this problem. Thank you.

0 件の賞賛
返信
1 返信

1,995件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Do you want to use CodeWarrior to connect to the target board to do Linux Kernel debugging?

If yes, please refer to CodeWarrior configuration in section 3 in this document.

https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-bo...

0 件の賞賛
返信