LS1046A Development on the LS1046ARDB using CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A Development on the LS1046ARDB using CodeWarrior

ソリューションへジャンプ
3,324件の閲覧回数
Daves_Garage
Contributor IV

Using Codewarrior, I am able to build a QorIQ Configuration Project for the PBL, and upload the RCW from the development kit.  Now I modify this RCW to disable the SerDes (or something), then compile the project, which generates a bin file in the "Generated_Code" directory.  If I use this file and update flash with it, it's endianness is wrong the next time I read it.  Is there an automated way from within CodeWarrior to fix this, or is it something we do manually.

I notice there is a utility in the LSDK when building this stuff from the command line.

Any pointers helpful.

Thanks.

0 件の賞賛
返信
1 解決策
3,200件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

No method in CodeWarrior to do this.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,252件の閲覧回数
Daves_Garage
Contributor IV

Yes.  This was exactly pointed out in my question above.  "I notice there is a utility in the LSDK when building this stuff from the command line."

I am aware of the python script for building the rcw, and generating the bin file.  My question is specifically about programming the RCW from within the CodeWarrior software.  Using the flash utility and flashing the bin file generated from CodeWarrior doesn't account for the big-endian ordering.  The question I need answered is:  Is there a method or process within CodeWarrior for doing this?

0 件の賞賛
返信
3,201件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

No method in CodeWarrior to do this.

0 件の賞賛
返信
3,254件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could use rcw package provided in LSDK.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw.git

$ git checkout -b LSDK-21.08 LSDK-21.08

$ cd rcw/ls1028ardb

$ ../rcw.py -i R_SQPP_0x85bb/rcw_1500_gpu600.rcw -o R_SQPP_0x85bb/rcw_1500_gpu600.bin

 

 

0 件の賞賛
返信