LS1046A Development on the LS1046ARDB using CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A Development on the LS1046ARDB using CodeWarrior

跳至解决方案
3,334 次查看
Daves_Garage
Contributor IV

Using Codewarrior, I am able to build a QorIQ Configuration Project for the PBL, and upload the RCW from the development kit.  Now I modify this RCW to disable the SerDes (or something), then compile the project, which generates a bin file in the "Generated_Code" directory.  If I use this file and update flash with it, it's endianness is wrong the next time I read it.  Is there an automated way from within CodeWarrior to fix this, or is it something we do manually.

I notice there is a utility in the LSDK when building this stuff from the command line.

Any pointers helpful.

Thanks.

0 项奖励
回复
1 解答
3,210 次查看
yipingwang
NXP TechSupport
NXP TechSupport

No method in CodeWarrior to do this.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,262 次查看
Daves_Garage
Contributor IV

Yes.  This was exactly pointed out in my question above.  "I notice there is a utility in the LSDK when building this stuff from the command line."

I am aware of the python script for building the rcw, and generating the bin file.  My question is specifically about programming the RCW from within the CodeWarrior software.  Using the flash utility and flashing the bin file generated from CodeWarrior doesn't account for the big-endian ordering.  The question I need answered is:  Is there a method or process within CodeWarrior for doing this?

0 项奖励
回复
3,211 次查看
yipingwang
NXP TechSupport
NXP TechSupport

No method in CodeWarrior to do this.

0 项奖励
回复
3,264 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You could use rcw package provided in LSDK.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw.git

$ git checkout -b LSDK-21.08 LSDK-21.08

$ cd rcw/ls1028ardb

$ ../rcw.py -i R_SQPP_0x85bb/rcw_1500_gpu600.rcw -o R_SQPP_0x85bb/rcw_1500_gpu600.bin

 

 

0 项奖励
回复