Kinetis KE02 ADC Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis KE02 ADC Configuration

1,642件の閲覧回数
taimurwajad123
Contributor III

Hello All,

I'm trying to configure KE02 ADC to measure voltage levels from GPIO. I'm using code warriors with processor expert. I have added ADC_LDD and currently trying to measure input from a single channel.

The code is compiling just fine without errors, but I'm not getting any output, and my variable is constantly zero.

Anybody used KE02 ADC, please comment.

Any help shall be highly appreciated.subra153

ラベル(1)
0 件の賞賛
返信
1 返信

1,520件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Taimur wajad ,

There is example code for ADC under "Help on Component" , I recommend you firstly test it , check whether it can work well.

pastedImage_1.png

also make sure the pin on board connect to signal is right . and  also check the signal.

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信