Kinetis KE02 ADC Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KE02 ADC Configuration

1,660 Views
taimurwajad123
Contributor III

Hello All,

I'm trying to configure KE02 ADC to measure voltage levels from GPIO. I'm using code warriors with processor expert. I have added ADC_LDD and currently trying to measure input from a single channel.

The code is compiling just fine without errors, but I'm not getting any output, and my variable is constantly zero.

Anybody used KE02 ADC, please comment.

Any help shall be highly appreciated.subra153

Labels (1)
0 Kudos
Reply
1 Reply

1,538 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Taimur wajad ,

There is example code for ADC under "Help on Component" , I recommend you firstly test it , check whether it can work well.

pastedImage_1.png

also make sure the pin on board connect to signal is right . and  also check the signal.

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply