Is the codewarrior v6.3 working ok with windows 7 x32bit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the codewarrior v6.3 working ok with windows 7 x32bit?

1,234 Views
michalistrapeza
Contributor II

Is the codewarrior v6.3 working ok with windows 7 x32bit?

Labels (1)
1 Reply

1,110 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Michalis Trapezaris:

Officially CW v6.3 was not tested under Windows 7-32 bits, but it works OK. I have used it like this for a long time and I have seen very few issues.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply