Is the codewarrior v6.3 working ok with windows 7 x32bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the codewarrior v6.3 working ok with windows 7 x32bit?

1,204件の閲覧回数
michalistrapeza
Contributor II

Is the codewarrior v6.3 working ok with windows 7 x32bit?

ラベル(1)
1 返信

1,080件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Michalis Trapezaris:

Officially CW v6.3 was not tested under Windows 7-32 bits, but it works OK. I have used it like this for a long time and I have seen very few issues.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信