Installing codewarrior development studio MPC5xx edition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing codewarrior development studio MPC5xx edition

2,255件の閲覧回数
Khushi
Contributor I

We have purchased a floating license for Codewarrior Development Studio and currently trying to install the MPC5xx Edition, Version 8.7 in which we are getting an error even after downloading the application from the official site. The error mentions ,
"

The contents of this file cannot be unpacked. The executable you are attempting to run has been corrupted. Please obtain another copy of the file, verify it's integrity and try again.

"
If anybody has faced a similar error, give the way out. Any help will be appreciated.
Many thanks in advance.

Best regards,
Khushi.

0 件の賞賛
返信
2 返答(返信)

2,173件の閲覧回数
Khushi
Contributor I

Hi Lukas,

There was a bit of misunderstanding after clearing which we led to a conclusion that the "Codewarrior for Microcontrollers (Eclipse IDE) v11.1" is the perfect fit based on our requirements. Thank you for your support.

Best regards,
Khushi

0 件の賞賛
返信

2,219件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Khushi,

which version of Windows do you use? Please notice that CodeWarrior 8.7 is old one and it's supported up to Windows XP only. If you have newer version, it won't work. There are no plans to provide update for this CW because MPC5xx are not recommended for new designs.

Regards,

Lukas

0 件の賞賛
返信