In the CodeWarrior v10.6  program the "New MQX 4.1 project" option is not displayed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In the CodeWarrior v10.6  program the "New MQX 4.1 project" option is not displayed.

1,222 Views
analattuca
Contributor I

Hello

I have a board TWR_K60D100M, when connected to USB port of PC I can update firmware with the soft "P&E Firmware Update".

Software PC:

- Windows 7 32-bit

- CodeWarrior for MCU Version: 10.6

- MQX4.1

 

Installed in the following order

1- OSJTAG firmware and drivers

2- CodeWarrior V10.6 (kinetis)

3- MQX 4.1.1

 

In the CodeWarrior v10.6  program the "New MQX 4.1 project" option is not displayed.

I compiled the MQX libraries for board TWR-K60D100M, but the "New MQX 4.1 project" option is not displayed.

 

What should I do to view this option?

 

Ana

Labels (1)
0 Kudos
Reply
1 Reply

1,099 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Ana,

Please make sure that MCU 10.6 updates for MQX are installed:

pastedImage_0.png

To install them go to Help -> Install New Software.. -> On the drop down menu select "--All Available Sites--" -> Select all the "MCU v10.6 Updates for MQX" -> Click on "Next"

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply