Where is expert mode view in Processor Expert, I can only see Basic and Advanced (CW10.6)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is expert mode view in Processor Expert, I can only see Basic and Advanced (CW10.6)

2,283 Views
russellsher
Contributor III

Hi

In the Component Inspector - where is Expert View as described by Erich in his article at:   http://mcuoneclipse.com/2012/11/12/tutorial-bits-and-pins-with-kinetis/

I only have the views as shown in the attached pic (view1)

Labels (1)
0 Kudos
Reply
2 Replies

2,112 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Russell,

In Processor Expert for CodeWarrior 10.6 there has been an update, the "Advanced" and "Expert" options were merged into one "Advanced" view mode so you will see there all available settings.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,112 Views
russellsher
Contributor III

Many thanks

Russell

0 Kudos
Reply