Hello
I have a board TWR_K60D100M, when connected to USB port of PC I can update firmware with the soft "P&E Firmware Update".
Software PC:
- Windows 7 32-bit
- CodeWarrior for MCU Version: 10.6
- MQX4.1
Installed in the following order
1- OSJTAG firmware and drivers
2- CodeWarrior V10.6 (kinetis)
3- MQX 4.1.1
In the CodeWarrior v10.6 program the "New MQX 4.1 project" option is not displayed.
I compiled the MQX libraries for board TWR-K60D100M, but the "New MQX 4.1 project" option is not displayed.
What should I do to view this option?
Ana