In Codewarrior 10.5 the source code is missing for ARM libraries in Cross_Tools  folder (arm-none-eabi 4.7.3) Where can I find it ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In Codewarrior 10.5 the source code is missing for ARM libraries in Cross_Tools  folder (arm-none-eabi 4.7.3) Where can I find it ?

2,771件の閲覧回数
thoborawski
Contributor II

In Codewarrior 10.5 the source code is missing for ARM libraries in Cross_Tools  folder (arm-none-eabi 4.7.3).  I would like to include the source in our current project.

 

According to my map file, the library

 

c:/freescale/cw mcu v10.5/cross_tools/arm-none-eabi-gcc-4_7_3/lib/gcc/arm-none-eabi/4.7.3/armv7e-m/fpu\libgcc.a

 

provides the following files to my project:

 

_arm_addsubdf3.o
_arm_muldivdf3.o
_arm_cmpdf2.o
_arm_fixdfsi.o
_arm_truncdfsf2.o
_lshrdi3.o
_ashldi3.o

 

Codewarrior 10.5 did not ship with the source code for libgcc. Can you post the source (a GNU requirement by the way) or at least tell me where to get it. Thank You

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,609件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Borawski,

Freescale uses GCC compiler in CW but we dont use GCC libraries. We use our own EWL (Embedded Warrior Libraries) and we provide the code of them in the following path:

C:\Freescale\CW MCU v10.6\MCU\ARM_GCC_Support\ewl

Best regards,

Carlos Musich

Technical Support Engineer

0 件の賞賛
返信

2,609件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Sorry for delay.

I've checked with development team and the source files you're looking for were not delivered.

Last year a new Kinetis development tool chain was released: KDS.

The KDS V2.0 is the last version released 2 months ago.

This development tool is using GCC too.

On this version all source files are delivered (not files you're looking for).

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信