I purchased a set of MPC5554 development kit, using the codewarrior2.1 version of the IDE, the suite comes with MULTILINK Rev. C debugger can be normal debugging. But I also bought the MULTILINK Rev. D debugger debugging process error, see the picture. Ho

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I purchased a set of MPC5554 development kit, using the codewarrior2.1 version of the IDE, the suite comes with MULTILINK Rev. C debugger can be normal debugging. But I also bought the MULTILINK Rev. D debugger debugging process error, see the picture. Ho

1,346件の閲覧回数
huafang
Contributor II
1 返信

1,249件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

this is rather question to PEMicro support. Could you please try to contact them directly?

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

Regards,

Martin